Hi,
We're using the BQ24257 in a new design. We are not using I2C for the time being. Plan is to have only stand alone node.
We have shorted the D+ and D- as we use DCP (5V 2A). Rlim is shorted to ground with zero ohm resistor. Riset is 127Ohm.
We have connected 3.7V Lipol battery to the BAT pins as shown in the attached schematics.
At present the I2C lined are pulled up to 3.3V and not driven by processor
L1 inductor used is given below
Vishay Dale | IHLP1212BZER1R0M11 | FIXED IND 1UH 5A 24 MOHM SMD |
System load is directly connected to VBAT as shown in the schematics.
When we connect the DC supply 5VDC 2A with D+ and D- shorted we are not observing any change on the battery voltage and there is no input current drawn.
But we could see LDO output at 4.9V. STAT pin is always high. We don't have NTC connected and there is a potential divider, one end of which is connected to LDO
Can you please advice on what could be wrong here?
Will it work without I2C? Is my schematics OK ? Is there anything wrong with the inductor selection?Batcharger1.pdf
Thanks for your response in advance
Thanks and Regards,
Seena