I am using a TPS54625 to power a 5V system. This is a consumer electronics product. When testing the product, I have noticed that an intermittent input power connection can cause the system to appear to have no voltage. I've done some testing and found that a short transient of no power after a successful power-up is apparently triggering the under-voltage latch (UVLO) and causing the part to shut down. Is there a solution to this (other than a crazy about of bulk capacitance on the input)?
Here is what a typical startup with a little noise looks like. The input voltage (yellow) is 13V roughly (minus a diode drop). The output voltage (blue) is set for 5.2V.
Even with a little noise it is fine. Also, it recovers fine if there is a large gap of no input voltage such as this:
Notice that it stops providing output, but when the voltage is again asserted, the system restarts.
But short gaps in the input voltage -- in the case caused by connecting the unit to power with a clip lead and dragging the lead a bit causing an intermittent connection -- results in the system failing to product output after the input transient:
In this particular case, you can see there were two transients, but it happens regularly with a single transient in the same time range, 10-25ms or so. Any thoughts on how to prevent this from happening? The data sheet indicates that the UVLO function is non-latching, but this tends to make it look latching to me.
In the fail state, Vout is 0V, VREG5 is 5.47V and PGOOD is low.