This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS65185 / Absolute Maximum Rating of VDDH_D.

Guru 11170 points
Other Parts Discussed in Thread: TPS65185

Hi all,
I work at Japanese distributor.
Please let me know about VDDH_D's maximum output voltage of TPS65185.

VDDH_D voltage is written, 22V ± 2V to the data sheet.
This device can adjust VDDH_D by VDDH_FB with resisters.
VDDH_DIS absolute maximum voltage is 30V.
Our customers will 27V the VDDH_D.
However, VDDH_D's absolute maximum rating isn't written in datasheet.

Do you know the maximum voltage?

Best regard,

Y.Nagai