This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Choosing an efficient regulator switch for dac7563.

Other Parts Discussed in Thread: OPA140, DAC7563, OPA2140, TPS7A49, TPS7A30

Hi, I have the next DAC7563 design. I've got 3 dac7563, a total of 6 DACs with 6 opa140 to adapt the output signal from 0..5 volts to -5..+5 volts.

I need to feed  3 dacs dac7563 and the 3 opa2140 (6 opa140) and I'm not sure the most efficient way.

I dispose of a source of 12 Volts@1A(max) and I need the following voltages:

1º.- Va = +5 Volts to feed the 3 dac7563 and REF5025.

2º.-I though in use the ultralow-noise TPS7A49 (to get ultralow noise: +Vb = +5V) and TPS7A30(to get ultralow noise: -Vb = -5V) to feed the opa2140 ICs. But my big headache it is to choose an efficiently power switch to convert from 12Volts@1A(max) to 5Volt to feed the DAC7563 and REF5025 and another power switch to convert from 12Volts to +5V and -5V to feed the opa2140. Could anyone help me to choose this ICs?

Thank you so much. Best regards.

  • There are many possible solutions.  The first thing you need to figure out is how much load current you require for each output voltage.

  • Hi John,

    Thank you for you quick response.

    1º.- These DACs outputs are going to command the speed of 6 thrusters and according to the manufacturer the control signal has an impedance of about 2.5kΩ.

    Then when the output is V= 5 Volts:

    Imax = Vmax /R = 5V/ 2.5k = 2ma/thruster -> 12 mA the six thrusters.
    (From positive power supply)

    and when the output is V= -5 Volts:

    Imax = Vmax /R = -5V/ 2.5k = -2ma/thruster -> -12 mA the six thrusters. (From negative power supply)

    I'm not completely sure if the calculations must be done this way.

    2º.- According to the datasheet (Page 5), the power consumption of dac7563 in normal mode with internal reference off is maximum 0.5mA@5.5V -> 2.75 mWatts per dac7563, then 6 units * 0.5mA = 3 mA

    3º.- And the power consumption of the Vref from REF5025 is around:
    i) Vref from dac7563 (according to the datasheet page 5): 15uA. 6*15uA = 90uA
    ii) Vref from V- of the opa140: I@10k= (2.5 - .667*Vdac)/10k Imax (when Vdac = 0) = 2.5/10k = 0.25mA

    Total = 0.25*6 mA + 6*15uA = 1.59mA

    Total(1º + 2º + 3º) = 12mA + 3mA + 1.59mA = 16.59 mA

    Thank you so much.
  • Those output currents are generally a lot smaller than what I usually deal with (output currents in the 1 A to 12A range). I would suggest you input your requirements into the Webench design tool and see what it suggests.