Hi,
I am relatively new to power electronics and am designing a 200W step up isolated dc to dc converter. Input voltage is 20-50V supplied by a solar panel and output is anywhere from 280-410V.
I am considering a few topologies. I have a few requirements. Efficiency is my number one priority. Second is the amount of input filtering. Since I am dealing with a solar panel input source, I would like a topology that requires low input filtering. Output filtering is not as necessary since my load is a battery.
I am considering:
Active Clamp Forward (good effiiciency)
Half Bridge?
Push Pull (may require too much input filtering)
I am also interested in doing MPPT, but I am not sure if there are any IC's out there that have MPPT as well as a converter controller.
If anyone has any recommendation on a topology to use, it would be appreciated. Also, if there are any IC's along with your topology recommendation that would be very helpful.
Thanks!