Hello,
We are Using UCC28070 for 2.5kW Front end PFC Power .Sometimes PFC boost MOSFET fails during start up at Low line (100V). Used Design calculator. Attached is the schematics for reference. The Max Duty Cycle is set to 96.6%.The MOSFET will fail whenever there is a continues disturbance in mains power Like Loose connection Power Socket, or arcing in the inpt plug etc. Under Normal ON/OFF it will not fail.
Note: Enable PFC is Not used in the applications.