Hi all
Would you mind if we ask LM5007?
<Question>
Our customer would like to add capacitance at SD pin for the input voltage which is the extremely gradual rise.
(We think that the start up of the device will be unstable because of extremely gradual rise.)
So, do you have the experience of addtion of the capacitance at SD pin?
And then, the data sheet shows that Remote Shutdown Thresholds are 0.45Vmin,0.7Vtyp and 1.1Vmax.
Our customer uses Ron resitance 15kohm.
In this case, how much will Remote Shutdown Hysteresis be?
(Our customer hope that it(Hysteresis) is less than 40mV.)
Kind regards,
Hirotaka Matsumoto