This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[LM5117] Max output current

Other Parts Discussed in Thread: LM5117

Hello~

According to LM5117's "Description & parametrics" page (http://www.ti.com/product/LM5117#parametrics), "Iout (Max) (A)" value is "20".

And, also "WEBENCH® LM5117" tool has Iout range is upto 17A.

I think that this device will be able to flow the larger current (>25A) to changing the sensing resistor value.

If that does not, I'd like to know the reasons.

Thanks... C.W. :)