In all application notes and evaluation boards related to LM5045, the current limit is implemented by CT(current transformer).
Although in datasheet, it is written that is possible to use sense resistor, I couldn't find any LM5045 example circuit with sense resistor.
in my application, I used a 15mohm shunt resistor instead of CT to detect the current limit 16A. in overcurrent condition the voltage on resistor would be 0.250v.
which is multiplied on 3 using an opamp circuit. then is connected to the CS pin through a RC filter with fc=1.6MHz which is 8 times greater than f=200KHz (R=1K,C=100pF).
without output load the performance is good. But with the 40w light bubble as an output load, the CS pin goes above 0.75v and the LM5045 switches to hiccup mode.
In another test,I tied the RES pin to the GND and disabled the hiccup mode, but the CS pin surpassed the 0.75v level.
Is there any other parameter that I had to consider but didn't? what's wrong with my design?
the schematic and waveform of CS and RES pins are attached if it helps.
any help would be appreciated