Hi,
The datasheet mentions in Recommended operating conditions that maximum output capacitor is 47uF but in Figure 2 illustrates regulator stability using Cout =100uF.
It is possible to operate the TPS7A7001 with an even larger Cout than this? We need to add extra output capacitance somewhere between 600uF and 1000uF. Is this possible with TPS7A7001? If not, is there any hack that can be applied between the regulator and the capacitor to allow larger output capacitance?
Best regards,