Hi,
We have an application using LM22672MRE-5.0 to convert VIN (12 - 24 VDC) to output 5 VDC.
But this product also has the option to be powered by 5 VDC from USB or from a separate connector.
So the question is: With VIN floating, can SW be driven to 5 V without damage?
From other threads (e2e.ti.com/.../357881) I understand it is usual that the VIN will rise close to SW when doing this. That should not be a problem in our case. As soon as the decoupling capacitors on VIN are charged no more current would flow as VIN is created using a bridge rectifier.
Best regards
Christian