This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCC3813 Technical Information

I have been studying a way to design a 200W DC-DC power supply.
The main DC bus range voltage of the system is from 180 to 420 Vdc, and it is the input of the power supply. The output of the power supply is 24Vdc+-2%. The power supply needs to be isolated (forward, half-bridge or full-bridge).

In this way, is it possible to use UCC3813 to implement 2-Switch Forward Converter for this specific application?

If not, which one device from On Semiconductor for this application would you suggest?

Thank very much for your help,

Joabel