This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Parallel TPS54386 Channels for Higher Current

Other Parts Discussed in Thread: TPS54386, TPS65279

Hello,

I have a design that uses several TPS54386 IC's currently, and these drive two separate 3A (max) channels, driven from a 24V supply.

We would like to expand our design to include single channels capable of 5A (max). Since we already have TPS54386 IC's available and they are already used on our PCB, we would like to determine if it would be possible to effectively parallel the two channels of a single TPS54386 to achieve a 6A (max) current, and set the output voltage for both outputs on the TPS54386 using a shared feedback network.

Insight appreciated.

Thank you.