I'm building a simple switch for a 130A DC motor (locked rotor amps) and have purchased some NexFET power transistors (CSD18535KCS). I chose these for the low Rds value and high current. The Datasheet claims these transistors can work up to 200A (Id current)
My motor typically draws 65A under normal operating conditions but just to be safe and not melt these things, i'm paralleling 3-4 of these transistors together.
Question? I can only rely on the datasheet for...data... but in looking the terminal sizes, can they really work up to 200A? Seems a stretch.