This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS63020 getting hot when switch on, even thought there is not load

Other Parts Discussed in Thread: TPS63020

HI,

I have done a PCB with a TPS63020 who delivers 5.5v under Vin=3V-5.3V.

There are two question that i found when i test my PCB,

1, when the input voltage is high than 4.7V, the TPS63020 close, and not voltage is delivered.

2, when the input voltage is lower than 4.7V, for example, 4.5v,  the chip can deliver 5.5v, but the input current to the chip is above 1.5A even thought there is no load. At first, it can deliver stable 5.5v, but the chip is getting hot and hot, and for about 1 or 2s, the output voltage start to oscilation.

 The voltage of the pin is show below.

Wish for reply.