This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS65217 End of Charging



Hi,

We are using USB charging only and register values were set as :

REGISTER                OFFICIAL RELEASE        
PATH:                   0001 1101    0x1D       
CHGCONFIG1:             0011 0001    0x31       
CHGCONFIG2:             1010 0000    0xA0       
CHGCONFIG3:             0111 0001    0x73       

The charging current termination limit can be defined in the register CGHCONFIG3 like

TERMIF[1:0]

Termination current factor

00 – 2.5%

01 – 7.5%

10 – 15%

11 – 18%

NOTE: Termination current = TERMIF x ICHRG

And charger termination is enabled on CHGCONFIG1 as

TERM

Charge termination on/off

0 – charge termination enabled, based on timers and termination current

1 – current-based charge termination will not occur and the charger will always be on

Charging current was set to 400mA (ICHRG[1:0], bits 7 and 6 in CHGCONFIG3),  charging voltage to 4,2V V(OREG[1:0] bits 5 and 4 in CHGCONFIG2) ,and termination current to 7,5%, as my understanding the charging should stop at 30mA current, but however it just continues until ~7…9mA.  Error in calculations can’t be blamed as external current meter presents same value to TPS65217.

Whether there is still some other registers impact this we need to consider?  

CHGCONFIG3 confirmed set as 73h. 

best regards,

Aslan