This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Qmax question

Hello,

I am working with a Lead Acid 12V 18Ah battery. In order to put an initial value into Qmax Cell 0 field, what value should I use: 18000 or just 3000 (18000 / 6 (series cells))

I've tried with 3000, but then the Full Charge Capacity value stays in 3000mA, which is wrong (if it refers to the battery capacity).

Thanks in advance.

Joao