Hi,
I just did a prototype using TI BQ25890 charger, there are some issues that I am encountering and I hope to hear your suggestions.
When I connect the Quick Charge USB adapter to the input of BQ25890, the handshake can successfully initiate and the voltage would change from 5V to 12V (which is good).
I also can measure good output (12V) at the PMID and good output (around 6.7V) at the REGN.
____________________________________________________________________
However, the voltage at the System Output and Battery + is completely off.....
The voltage at the Batt+ is 1.75V and Sys_out is around 2.4V.
Also I noticed that the Sys_out is very noisy.
Below is the my circuit schematic:
Since the Batt+ voltage is lower than the voltage of my battery, the battery isn't charging.
Also, another observation is that the Vin would switched to 5V as soon as I connect a 3.6V battery to the circuit.
If I remove Vin and the battery stays connected to the charger, I get a healthy and clean output at Vsys and PMID.
Seems like the problem is with the buck converter of the charger. Any thought on what I should do to isolate the problem?
Thank you so much,
Jeff