Dear, All
I have a question about current limit of BQ24190.
Question 1
The OUTPUT current of Isys(4.5A) is listed in "Recommended Operating Conditions" of the data sheet, where is the limitted circuit?
Question 2
"Discharging current with internal MOSFET "of Ibat is listed with 9A peek, where is the limitted circuit?
Is this limitted circuit same as Ibatfet_ocp(System over load threshold)?
Question 3
Please tell me for differences between Isys(4.5A) and "continuous(6A)" of Ibat(Discharging current with internal MOSFET).
Thanks, Masami M.