Hi,
My customer is evaluating the LM25117.
But the Lo-side driver works an incorrect operation when the SYNC frequency is dropped.
The waveform and condition is following;
- CH2(Green):High-side Gate voltage
- CH3(Red): SYNC signal
- CH4(Blue):Lo-side Gate voltage
- Oscilating Frequency:300kHz
- Sync Frequency:241kHz
- This work has a tendency to occur with the heavy load than the light load.
1. When On-state of the SYNC signal is longer than Off-sate, does the Lo-side driver works an incorrect operation ?
2. When the SYNC signal is Off-state more than fixed time, does the Lo-side driver works an incorrect operation ?
3. Is there any reason that the Lo-side driver works an incorrect operation?
If there is any lack of information please let me know.
Thanks and Regards,
Kuramochi