Hi Everyone,
Please let me ask about default register setting input Current Limit value. The table.9 in datasheet state the default value is 500mA (REG00[5:0]=001000) but I checked it by using EVM then the register value was 3.25A (REG00[5:0]=111111). So I think that there is typo in datasheet or the revision of device on my EVM is old so it has different default value.
Please check it and give your comment.
Best Regards,
Sonoki / Japan Disty