Hello,
While using a device in IBB configuration, I noticed that there is a bypass capacitor(IOC) from input to output. (Capacitor C4 in Figure 3 in http://www.ti.com/lit/an/slva257a/slva257a.pdf)
I have a couple of questions regarding this:
1) As per my understanding, when the device starts up, if VIN is ramped up from 0 to 18V, VOUT should jump to some positive value due to charge sharing between C4 and C3 before the device starts ramping VOUT down to a negative value. How is the initial rise prevented? I do not see it in the bench results(figure 6 in http://www.ti.com/lit/ug/slvu243/slvu243.pdf
2) Won't line transients cause severe overshoot and undershoot as the transient is passed through the IOC straight to VOUT?