This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Suspecting BQ78350 Balancing Loop

Other Parts Discussed in Thread: BQ76940

15S4P Li-Ion (NCR18650BD 3150mAh each)
AFE = BQ76940
Cell Balance Threshold    4000    mV
Cell Balance Window    100    mV
Cell Balance Min    40    mV
Cell Balance Interval    20    s
Balancing current ~325-400mA from 4V to 4.2V

 

That's actually the first time one of our pack gets into balancing and I have the feeling there is something wrong.
Balancing had been going on for roughly 45 minutes while charging (near 100%).  Soon after I removed the battery from the charger, the balancing stopped.  

A few minutes after, I put back the battery to charge.  Balancing did not start and valid charge termination occurred in less than 10 minutes.

It turns out that the small unbalance I had noticed on one cell was reduced well under the unbalance threshold. So, something worked, but it looks like I had to break the loop.

Could the balancing current be too high or the thresholds badly set?

What are your thoughts?

Regards,

Frederic