I am using the BQ29701. I have it hooked up as in the sample simplified schematic. I have not included the resistors to Cout and Dout, but rather just the resistor, capacitor between the terminals and a resistor from V-. Everything was working as expected for about a month on a 19mA hour Lipo battery. It was then that I switched to a similar battery, but different brand. Now when connected, the battery will not go high.
I can force it high by temporarily shorting the battery to ground and then it will stay high for a time (before randomly going low again). It is on a jumper as well, so I can not disconnect and connect the jumper and expect it to stay high. It then needs shorting again. I saw in the datasheet that on the first time it may need to be shorted to ground so I am wondering if this has something to do with it.
I have also tried changing back to the old battery as well as a different battery with no luck. The problem persists (on three seperate boards). I have disconnected from the rest of the system, so the power is just going to an LDO and nothing else. I am also curious if the need to short to ground is common. This seems like a hassle for manufacturing on small boards.
Thanks,
Nick