This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SMPS or Flyback Help Develping



Hello,

My goal is as follows.
Vin: 3.7 - 4.2 (single cell 18650 battery 2500mAH 25A)
Vout: 3 - 5
max Amps out: 10
I will be connecting a small heating element 2mm x 8mm in resistances from 0.2ohm to 1.8ohm. I would like to control the power setting from my Arduino.


Thank You, John