This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM2576-5.0 with max ILoad = 50mA

Hello,

we use the LM2576-5.0 with VIN = 24VDC and the ILoad is now min. 27mA and max 50mA.

Now we could not found the minimum Load Current in the DataSheet Document.

We only found the Test circuits with 0,5 <= ILoad<=3A.

My Question: Works the LM2576-5.0 correct with 27mA and 50mA?

Is the Load with 27mA and 50mA enough?

Thanks and best regards

Stefan Balck