I have a TPS65910A3A PMIC driving an Am3352 with a single x16 DDR3. Most of the voltages out of the PMIC are good except VDDIO. It should be +1.5V and it is only +0.94V. This occurs on multiple boards. I've connected the PMIC with the Am3352 almost identically to the TMDSSK3358 and TMDSICE3359 schematics.
VBAT and VBACKUP are +5.0V. Boot1 is connected to PMIC_VRTC, Boot0 is connected to ground. PMIC_VRTC is not connected to anything else. PWRHOLD is connected to +5.0V and PWRON is pulled up to +5.0V and connected to a push button. The RTC is not used so OSC32KIN is connected to ground and the OSC32 and CLK32 outputs are open. nRESPWRON goes straight to the Am3352 PWRONRSTn. The pcb has a ground pad under the PMIC and I believe the PMIC is soldered to the pcb pad. I have all the recommended capacitors (2.2uF, 4.7uF, 10uF) and inductors (2.2uH) that are in the reference designs.
VDDIO powers the Am3352 VDDS_DDR, the DDR3 VDD, and a TPS51200 VLDOIN. The TPS51200 provides DDR_VREF to the Am3352 and DDR3 and VTT to the DDR3 termination resistors.
VDD1 and VDD2 are both +1.10V. VDIG1, VDIG2, VAUX1, VPLL, VDAC, and VRTC are all +1.8V. VAUX2 and VAUX33 are +3.3V. BUT VMMC is +3.7V, which is another problem.
Any insight as to where the problem is would be appreciated. Any suggestions where to look?
Thanks.
Burt.