Hello
I have a BQ25890EVM-664 connected to an EV2400.
If communications is established with the board, the CE line coming from the I2C interface is high (non-assert), and the charge is suspended. There is a CE check box on bqStudio, but if it is either checked or unchecked, an error message appears "Error Code: 53 Msg: EV2x00 operation specified is not supported".
I have tried independantly asserting CE and charging resumes, but there is then no communication with bqStudio.
Has anyone experienced a similar problem?
Thanks
Doug