This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Ev2400 and BQStudio, automated / manual learning cycle

Other Parts Discussed in Thread: EV2400, BQSTUDIO

Hello again,

another problem:

using BqStudio / EV2400 (Firmware0.18), selecting Learning Mode, Automated Mode: setting Load Control Pin to VOUT1 and click Test , BqStudio shows me in the lower left corner of the window "EV2X00 operation specified is not supported" and the VOUT1- Pin on the Ev2400 does nothing ? What does that mean ? It should set my VOUT1- Pin to 5V right ?

Ok, its not working, tried manual mode, reading "... two relays which are connected to selectable Pins ..." BUT I cannot select any PIN ? How should I connect my EV2400 to run at least a manual learnung cycle ? (remember, automated mode WOULD be much better, BUT is not working (see above) ),


Any Ideas ? Thx in advance , Enrico