Hi,
Can someone tell me the difference between TPS22954 and TPS22953? Also, does TI have any current limiting load switches with Power Good feature?
Thanks!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Rohit,
The TPS22954 has quick output discharge (QOD), which discharges the output of the switch when the device is turned off. The TPS22953 does not have this QOD feature, but it has reverse current blocking when turned off. Please refer to the block diagram in the datasheet for a pictorial representation of this.
The eFuse portfolio may be closer to what you are looking for. These device come with current limiting as well as power good and other protection features. The TPS2420 is a 3V to 20V load switch with a 5A current max and adjustable current limit. Is this device closer to what you are looking for?
Thanks,
Alek Kaknevicius