This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ34Z100-G1 After Qmax calibration

Tom,

I manage a new calibration Qmax Cycle and at the end of the charge termination I watch strange values for the following parameters :

  • In data FLASH, Qmax Cell 0 : 7339 mAmpHr
  • In the registers, Remaining Capacity : 339 mAh
  •                               Full Charge Capacity : 339 mAh

Is there a procedure to make a complete re-initialisation before a Qmax calibration ?

Thank you for the answers

Mickael