Hi,
I am using BQ25504 for harvesting energy from a 3V (Voc) 150mA (Isc) Solar panel to charge a 3.7V, 680mAh Li-Po battery. I made a prototype PCB based on the application circuit given in the data sheet with the following design conditions,
VBAT_OV = 4.2V VBAT_UV = 3.0V
VBAT_OK = 3.3V VBAT_OK_HYST = 3.7V
VIN_DC = 3.0V VREF_SAMP = 2.34V
I used (SLURAQ1 excel calculator for selecting resistors.
For the purpose of testing, I connected a Li-Po battery (charged, around 3.72V) to the VABT pin and set VINDC = 1V using a DC supply. The circuit draws 20mA from the DC source. I kept this running for around 4 hours. When I checked after that, VSTOR is found to be 0.951V and VBAT_OK is 0V. I tried increasing VINDC and saw that at VINDC = 2.117V ,VSTOR = 1.8V and current drawn by the circuit is 6mA and at VINDC=2.38V(~VREF_SAMP) VSTOR is connected to VBAT and I get 3.72V at this pin and 3.7V at VBAT_OK pin. Now, the circuit draws current only in uA from the DC supply and it is not charging the battery even if I decrease VINDC below 2.38V. In short, I couldn't get the device working as expected.
Is there anything I am doing wrong?Can any one give me a hand with this?
Thanks
Priyesh