Other Parts Discussed in Thread: BQ24650
Hello All,
I attempted to design in a charger circuit for our 19.2V (6S2P) 6000ma/h battery packs. We currently use a desktop off the shelf charger to do this running 22.2V max 4A. The idea is to build the charger into our PCB using the BQ24650 for various reasons I wont get into.
We want to charge at 22.2V max 1A using this circuit, and of course the 1A would reduce if the MPPSET falls below 23.5 VDC (as set in our case).
Our supply voltage is a max of 28VDC without load.
When the Vin has power applied, battery unplugged, it draws 5ma and stat1 is low, stat2 is high, indicting a charge in progress.
When the Battery is plugged in, no change....stat1 is low showing a charge in progress but still only drawing 5ma.
The voltages I read on the pins with the battery plugged in are:
VREF: 3.297V
MPPSET: 1.94V
REGN: 5.95V
HIDRV 19.7V (the scope shows some PWM here)
PH 19.7V (which is the battery voltage level plugged into the circuit or unplugged
LODRV 0V (no PWM)
SRP/SRM 19.7ish VOLTS too close to read the difference using my multimeter
VFB 1.873V
I can scope a pwm like shape on the HI side mosfet Source pin around 19.7V and after the inductor a nice smooth 19.7V.
Anyways it is just not sending any sort of charge into the battery. I waited much past the 30 min 1/10 charge recharge phase, but not different, just the 5ma most likely for the lit up LED. Any idea what the issue could be?
Thanks in advance,
Jeff