This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

About DCV0105 Series

Hello.


My customer is currently in use DCV0105 Series, I have gotten a question about this product .

So , I have a question about DCV0105 Series.

<Question>

◎What are the things that becomes the factor that determines the characteristics of the "Output Voltage vs temperature"?

( For example , "Vf" characteristics of the internal diode ? Or , Do you have one that caused something other also ? )

Could you help us?

Best Regards,

Masumi Sekiguchi

  • DCV0105 thermal data / temperatures is determined by the only active control device internal of this package,

    DCV01xxx series operating temperature range is-40°C to +85°C.

    Junction to case (Theta JC) =26°C/W power dissipation

    Junction to Air( Theta JA)=61°C/W power dissipation

    Tom