This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS61087 Input current

Other Parts Discussed in Thread: TPS61087

Hi,

I am using TPS61087 boost LED driver using which 4 LEDs has to be driven. The LEDs are divided as two groups, each consisting of 2 LEDs in series and the groups themselves are commonly connected parallel to the output. Each LED's forward current is 80mA and forward voltage is 2.9V. How can I know the input current consumed by the driver? (in case the description is obscure, consider that the LEDs' forward current is 80mA  and forward voltage is 5.8V)

Thanks,

San.