This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ27520 EVM Rev A

Other Parts Discussed in Thread: BQ27510, BQSTUDIO

Hi,

I am using a q27520 EVM with EV2300. The problem that I am facing is that the current measured is  negative times the actual current (-1*Actual Current). If I am charging the battery, I am seeing negative current and while discharging, I am seeing a positive current in the software. As per the calibration definition in bqeasy, discharging current is supposed to be negative and charging current should be positive. I have used bq27510 module previously and therefore, I am certain that the definition of bqeasy is correct and therefore the discharging current should be negative. 

eg: if the battery is being charged by 300mA, I am seeing the current as -300mA in the software.

Can somebody tell what is going wrong?

  • Hi Akshay,

    pls use bqstudio instead downloadable from ti.com. Make sure to calibrate the cc and board offsets as well as current. This should fix your problem.

    thanks

    Onyx

  • Hi,
    I have tried using bqstudio as well. But, the problem remains the same. I have tested it after calibrating also. Calibration is for offset correction from what I understand. What I observe is that the gain of the equation is being taken as -1*Req_Gain. Right now, I have not even applied any load. I am just charging the battery using power supply where Charger+ is connected to V+ on supply and Charger- on V- supply. I can't test with reversing the connections since my battery has no protection circuit.
    Please let me know if there is any other way to fix this.
    Thanks
    Akshay
  • Akshay,
    The problem is that you didn't carry out current calibration correctly. calibrate the current using a positive current . Make sure the current across the sense resistor is going from cell - to pack - (which is indicative of charging) and not the other way around.

    thanks
    Onyx
  • Hi Onyx,

    It did solve my problem.

    Thanks!

    Akshay