I followed all the steps. Connected the USB dongle to the board, powered up at 12V, TI software found the board and connected to the dongle. Power on all the outputs came up but was not the values on the GUI. 3.3, 2.5,1.8, 1.2
Have not applied a load to any of the outputs.
I tried adjusting the output voltage on the 3.3V with apply changes immediately selected. No change on the output according to my DMM. Did a soft reset and the output went unstable.
Closing the SW and re-opening the software brought the 3.3V back but still no control and soft reset makes it lose it's mind.
Tried setting the EEPROM value to default. Still no change in behavior.
Is there a validation procedure or video I can follow for the EVM itself?