Hi,
I have one question for TPS659037.
I would like to ask the unused pins handling regarding VPROG, I2C2_SCL_SCE and I2C2_SDA_SDO.
1) VPROG :
According to the Pin Functions in data manual ( slis165a) , it is written in the below.
・Ground or floating @ primary function: OTP programming voltage
・Floating: @ secondary function: TESTV
Also according to 2.9.1 VPROG in the design guide (slia088), it is written in the below.
VPROG is only used for factory testing, and should be left floating.
Which handling is correct, Ground or floating? Our customer connected to the Ground. Is it problem?
If it is problem, please let me know what matter is.
2) I2C2_SCL_SCE, I2C2_SDA_SDO :
According to the Pin Function in the data manual (slis165a), it is written in the below.
・Floating
Also according to 2.6.6 in the design guide(slia088), it is written in the below.
・If I2C2 is unused, both I2C_SCL_SCE and I2C2_SDA_SDO lines should be either pulled up to VIO, or
connected to the I2C1 lines.
Which handling is correct, Floating or pulled up to VIO? Our customer keeps Floating. Is it problem?
If it is problem, please let me know what matter is.
I appreciate your quick reply.
Best regards,
Michi