Hey all,
I'm looking for some professional feedback on my schematic based around the LM3409. I used the WEBENCH tool for the majority of the components. The inputs were 12-42V, 3S Cree XM-L @ 2.7A, and 30C ambient.
In order to create two modes (given two 12V signal inputs) I added a pair of relays and a normally closed solid-state relay on the I_adj pin. The idea being that when the "high" signal turns on, the relay will open and give full power. Without the high relay, "low" mode is adjusted using the 50k trimpot. My calculations show that this should give dimming ability from around 0-20% of full power.
Would it be possible to take a glance at this concept before I move forward and lay out a board? Are there any issues with using a SSR for the I_adj pin that I might be missing? Any input would be awesome! I look forward to using this driver in my designs and want to make sure the theory is right.
Schematic: http://i.imgur.com/DxYuYcq.jpg