This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM3478 Design, noice

Other Parts Discussed in Thread: LM3478

Hi,

I have a new design for the LM3478.  Vin: 11...13V, Vou: 33V, Iout 0...250mA.

I ussed a 390uH coil. Cin = 30uF, Cout = 33uF. Rloopcomp: 100R, Cloopcomp: 10nF.

RFA: 100K, Comp: 27K + 2n2

Running so fahr well.

Problem: noise in in different areas of the Current from 0 ... 250 mA.

I changed Rloopcomp from 100 to 4K

I changed Comp with different values.

What can I do ?

Thanks a lot.

Best regards

arnold zender