This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS2554DRCR - About this device based on “EN 60950”

Guru 21045 points
Other Parts Discussed in Thread: TPS2554, TPS2544

Hi Team,

 

I understand that TPS2554 is based on “UL standard”.

Please refer to a URL as follows.

http://database.ul.com/cgi-bin/XYV/template/LISEXT/1FRAME/showpage.html?name=QVGS2.E169910&ccnshorttitle=Protectors,+Low-voltage+Solid-state+Overcurrent+-+Component&objid=1075449610&cfgid=1073741824&version=versionless&parent_id=1074427572&sequence=1

 

So, is this device based on " EN 60950"?

Could you please let us know if you have any information?

 

Regards,

Kanemaru