Hi,
I have to manage a linear regulator to convert 12Vdc to 5Vdc with a maximum current of 150mA. I had a look to the file ISO3088, and the TPS7A49 option It could be a good option but I'm not pretty sure if it's going to be too much current to be dissipated because I'm going to have a drop voltage of 12-5 = 7V.
I don't like to use a buck converter because I'm going to use the 5Vdc branch to feed DACs an ADCs.
It doesn't mind to use two linear regulators instead two to try to dissipate better the heat.
Two TPS7A17 It could be a good option too.
Could anyone give me a recommendation to this issue?
Best regards.