I've recently been working with the TSP40211 to produce an LED panel driver. To the eye the output is perfect, however this is to be used as a film light and there is noticable flickering even though the LED PWM output is set at 500KHz.
Is there anything I can do to resolve this problem and get rid of the flicker?
So far I have tried adding the 10uF electrolytic capacitor to try to smooth the output, and I have also tried a 100uF but with no success.
Here's the current schematic.