Hello, this is the first time I've used WebBench for circuit design recommendations.
I set my criteria as follows:
Vin: 16 - 30 VDC
Vout: 24VDC regulated
Iout: no more than 5Amps.
With the input above, the recommended part was the LM25118. It's rated to source 20Amps, as a result, the components are very, very large.
Can someone guide me to a more "size appropriate" design?
Thanks, Brian