Hi team,
I'm looking for a part with the following specs AND that contains an available EVM.
- VIN: 38V
- Vout: 8V - 24V
- Iout: 3A
No need for any extra external controls like Enable, SHDWN, Adjustable Current Limit, Selectable Switching Freq., etc...
The closest thing I was able to find was the LM22670. I'm confused about the EVMs output voltage. I've noticed that several EVMs have a 3.3V and I believe the output voltage is adjustable on this part.
- Is the 3.3V fixed or can it be adjusted on the EVM?
Thank you all for your help,
Mauricio Solis