This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ25570 - minimum operation current

Other Parts Discussed in Thread: BQ25570

Hi all,

Would  you mind if we ask BQ25570?

Our customer uses the BQ25570 as following condition;

<Our customer's condition>
Vin : 2.7V, 2.3mA over
Vout : 3.3V or 3.6V

We have one question about minimum operation current of BQ25570.

When Vin current is less than 2.3mA, Vout belows to 2.0V(@2.7mA).
(in case of less than 2.3mA, it is not possible to output normally)
So, how much is minimum operation current in case of Vin=2.7V? 488nA?

Kind regards,

Hirotaka Matsumoto