I'm using a BQ24450 to charge a 12V 2AHR battery, that acts as backup when the AC fails. Everything works as it should. Float voltage is set to 13.5V
This circuit has a load connected to battery at all times, that draws about 150mA, occasional drawing up to 350mA for shorty bursts. The DC power supply that powers the BQ24450 can deliver 1A@15V
Will having the load connected to the battery cause any problems for the charge algorithm? The sense resistor (pins 2,3) will obviously see the charge current as well as the load current.