This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

About soft start at TPS53315.

Other Parts Discussed in Thread: TPS53315

Dear support member,

My customer use TPS53315.

At the resistor connected to the MODE pin,
recognize that I can set the soft start time.

When connected via a 100kΩ to PGOOD pin,
What percentage of about ± with the exception of the resistance error or will those that occur?

Could you teach a formula to realize the 1.4ms with a resistance of 100kΩ?


Best Regard.
Bob Lee.