Hi,
Can I put my power adapter parallel to the battery? I put my input and battery terminal connected then does it affect charging status of the battery? If I use common cathode diode to isolate the input power or battery power to the system load then does it affect the system ?
And what is meaning of this line given in datasheet:
A system load can be placed in parallel with the battery as long as the average system load does not keep the battery from charging fully during the 10 hour safety timer.