I was able to successfully program the data flash portion of my bq34Z100-G1 devices using the 'golden rom' image generated by the EVM software from my application running on my target system. Prior to using the block programming method in document SLUA665 "Going to Production..." I had been messing about with trying to update individual flash locations and I think that I may have buggered up the program flash memory. Since I have both the firmware flash and data flash contents from my EVM board available where can I find the commands for programming the firmware memory? These don't appear to be documented anywhere. These devices are "in system" sitting on I2C1 of a AM3352 processor, and aside from some tricky micro surgery I have no way to attach something like a EV2300 to these boards for programming the blighters, I need my C application code to do this.
Regards,
-Jeff